This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What commands (and shell/environment?) are available in CCS pre- and post-build steps?



I'm trying to some custom build steps to build a project. I have done the more complicated bits (converting .out to .bin, combining two ELF files) using TI tools and some example variables but the last very simple step is a bit of a puzzler for me. I simply want to copy a file, to replace the normal project .out file with the combined ELF file. But how to do so in a cross-platform way? I want this project to work regardless if running under the Windows or Linux or macOS versions of Code Composer that are available.

Of course in Linux and macOS I could use `cp` assuming they are in the PATH or available at a known path like "/bin/cp".  Under Windows perhaps it would be `COPY` although looks like that is a DOS builtin and it's unclear whether CCS runs the build steps in a shell or parsing/executing them itself directly. And to do both I would need to do some sort of `if POSIX then … else if WINDOWS then …" logic which also opens questions of whether there is a shell language available to pre/post-build steps or at least what environment they run in. My impression so far is that:

* CCS is doing its own variable expansion first with its own syntax for things like "${CCS_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin" even though it looks like something compatible with a Unix shell

* probably just running directly, with the working directory set to the active configuration folder like "Debug/" and things like "pipes" or "redirection" or conditional logic is not available?

* if the tools are not installed with CCS (I only see `gmake` and `unzip` and `zip`) or with the SDK (like the ARM compilers and such) then I probably cannot rely on them cross-platform??

Is there documentation I should be referring to for these kinds of questions? The information at "6.1.3.4. Pre and Post Build Steps" of the Users Guide (currently found at https://software-dl.ti.com/ccs/esd/documents/users_guide/ccs_project-management.html#pre-and-post-build-steps although the link doesn't seem to take you directly to that section in prctice) is very high-level and doesn't really go into details like this.

  • Hello,

    The pre/post build commands work in a very simple way. CCS first expands any build variables, then it passes the entire string as-is to the system console and executed there. That is it. Pure cross platform will be tricky since the system commands and operations will vary depending on the host OS (Windows vs Linux). Shell scripts would also be system dependent (bat file on Windows, sh on Linux). 

    Hope that explains things

    ki

  • Thanks, yeah! Would have been a nice surprise if there was an easy way to do this, but good to confirm my understanding of the situation in the meantime.