This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CODECOMPOSER: CCS/USB560v2: Error -1060 whe debugging C6713B

Part Number: CODECOMPOSER


Hello,
I have a problem to debug a C6713B under CCS10.3.0 with a Blackhawk BH-USB-560v2 emulator. In addition to the standard installation, I have installed Code Generation Tools 7.4.24, as the newer tools do not support the CPU.
The operating system is Windows 10 (64 Bit version).
I have created the setup for the debug session. Executing "Test connection" delivers good results.
When I try to debug a project, I get the following error message:

TMS320C671X: Error connecting to the target: (Error -1060 @ 0x0) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.3.0.00042)

I have tried this setup with a hardware from a customer and also with the C6713DSK. Both show the same error. I have also tried with my laptop, which runs the same OS, and also got the same result.
A debug session with another CPU (C5509A) is working well on the same computer.
Thanks for your help.