This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have been trying to add the compiler version 20.2.1.LTS to code composer studio 8.3.1! I have installed the tool manually and the tool does not recognized the driver. I am out of ideas, I am running a 32-bit windows 7 machine. Also, I tried the CCS store, it did not work!
Hello,
I have installed the tool manually and the tool does not recognized the driver.
Please see the section "Compiler Discovery" in the below article:
Thanks
ki
Even after adding the path, the tool does not show the version! I was wondering if there was another issues.
Did you press the "Refresh" button?
Can you provide a screenshot of the Compiler dialog (please show the relevant data in the dialog)?
Thanks
ki
I found the issue, the drivers are not properly documented! ti-cgt-c2000_20.2.1.LTS compiler driver is only available for Code Composer Studio 10. They should document the drivers and Software needed together.