Part Number: CODECOMPOSER
Hi,
I want to ensure that a project is always built with the same CCS version.
I have created a project in CCS 10.1.0. I updated the CCS version to 10.2.0.00009. I changed the Code Composer Studio Version Validation option to "Error"
Then I sent the project to a build machine that has only a fresh installation of CCS 10.3.1
When I build the project in the build machine with 10.3.1 version, I don't get any error or warning related to the CCS version.
Where should it be shown?
Thank you very much,
Álvaro