The problem is loading error with CCS3.3 . The projet is built successfully but loaded symbols fail.
My compiler options=-g -q -pr -me -mv7a8 --abi=eabi
Linker options= eabi -e_c_int00 -heap0x800 -stack0x800 -w -x
My ccs version is 3.3.81.5 and tms470 tools is v4.6.3
This problem appear when I build this program and try to load *.out.
After delete the structure function ,problem will die out. I think if this is CCS bug and I'm desperate for a correct solution ,thanks!
Program as show below:
class CTest
{
public:
CTest(){m_pTest=0;}; // After delete the structure function ,problem will die out
int* m_pTest;
};
class CComEntity
{
private:
static CTest s_value[10];
}
CTest CComEntity::s_value[10];