I've been running CCS4 on the abovementioned system and I'm having trouble with the Project Properties window. It seems not to be providing me with options that should appear. I'd like to set up the Build process to provide assembly listings of the C code. Apparently this is supposed to appear in the C/C++ Build window as a set of options. However, this is what I see (image below). I thought I was supposed to see something else in this window? If anyone has any ideas, I'd welcome them. Not sure if my CCS4 install is corrupted? Other stuff seems to work - Build, load to target, run code on FET, etc.