Other Parts Discussed in Thread: CC2642R, SYSCONFIG
Cross posting from the CC2642R forum to this one:
Hello, I am currently working on porting the Adafruit GFX and EPD libraries from arduino to work with the CC2642. I read from previous forums that while C++ is not officially supported, it can be done. I am definitely new to porting libraries and I have run into an issue where a function is defined in a file that is auto generated by sysconfig in C, and is extern -ed in another autogenerated file in C as well. I need this function to work in C++ in my own file, and when I do the usual extern "C" func(); it will not work because it is extern -ed in C in the other file. I cannot edit the autogenerated files as every time I compile they are reset. I am wondering if there is a workaround that I can use or if I have to end up converting all the libraries from C++ to C. Attached below is the code. Any advice on how to port these libraries is also welcome!
Here is the code in my file and the error that it gives when I try to extern "C"
Here is where I run the function, and the error it gives when I do not have extern "C" in my file
Here is the other extern that is in the sysconfig auto generated file "ti_ble_config.h"