Hello,
I'm using CCS 10.3.1.00003.
This morning when I powered up CCS at the office after working at home on Friday it couldn't find some of the files in the project. One of the path variables seems to have been corrupted. I fixed the paths for the files and now the project compiles but I can't search the project. Additionally when using CTRL-H C/C++ Search or right clicking a variable and asking for Open Declaration no results are provided. Or in the case of the Open Declaration it jumps to the wrong location.

I've tried -clean and I've tried deleting the Metadata and reimporting the project. Neither worked.
One note: On Friday it kept showing an indexing issue. Today that's gone after I deleteted Metadata and reimported project.
Project is located on local drive that's backed up via OneDrive.
Any help would be appreciated
Thanks - Bruce