Hello, I use the CCS 4.2.1 to develop my software for the ARM9-Part. Operating system is SCIOPTA. A little demo program from SCIOPTA is running well. But my great program has the problem, that the source-File and the generated assembler commands does not correspond. See my code snip.
_start, _start, _c_int00:
0xC0012720: 0000E59F MULEQ R0, PC, R5
1386 cmp r0,#0
0xC0012724: FF30E350 .word 0xFF30E350
1388 blxne r0
0xC0012728: 1010112F ANDNES R1, R0, PC, LSR #2
1393 ldr r1,st_sc_sysProcDispatcher
0xC001272C: 0000E59F MULEQ R0, PC, R5
1394 cmp r0,#0
0xC0012730: FF11E350 .word 0xFF11E350
what can be the reason for this effect ?
best regards
volker