Part Number: CODECOMPOSER
Hi all,
Is there any way to find out what default build configuration is defined when launching CCS or importing a new project?
Does this default configuration applies always when importing the project? I have realized that if I
1.- change the current build configuration of the project
2.- remove project from workspace / close CCS
3.- launch CCS / lmport project again
...the project is not imported with the last build configuration established.
So I guess that there is a default build configuration.
By the other hand, I have realized that the chronological order when the build configurations are created, modifies the .cproject file. In fact, new build configurations are added after the old ones.
So it seems that the first chronological build configuration defined is the default one, but I am not sure at all. Because other colleagues with same CCS version and same project but different computers do not see the same.
Thanks in advance
Best Regards