This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS Version: 4.1.2.00027 and BLACKHAWK USB2000 Error



I just installed a floating license version of CCS4 (uninstalled old one, installed the disk that I just got).  I performed a local update.  I am using the TI LV MOtor kit. I configured the jumper to disable onboard jtag, so I can use the Blackhawk USB2000.   After I configured the targer for LV Motor kit and Blackhawk USb2000, I can no longer commuinicate with the LV Motor kit board.  I receive the following error:

C28xx: Error connecting to the target: Error 0x80000240/-603 Fatal Error during: Initialization, OCS,

What am i Missing?