Hello
I built a application for TMSF28379D using Code Composer 10.
I created Motor Controller project for CCS and 28379D.
Normal operation before adding code. but when i add some code, ccs do not build yet.
--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
This is my error
> Compilation failure
makefile:164: recipe for target 'Six_ph_control_cpu1.out' failed
"../2837x_RAM_lnk_cpu1.cmd", line 60: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. placement with alignment/blocking fails for section ".text" size 0x3a6cpage 0. Available memory ranges:
RAMM0 size: 0x2de unused: 0x0 max hole: 0x0
RAMD0 size: 0x800 unused: 0x0 max hole: 0x0
RAMLS0 size: 0x800 unused: 0x0 max hole: 0x0
RAMLS1 size: 0x800 unused: 0x0 max hole: 0x0
RAMLS2 size: 0x800 unused: 0x0 max hole: 0x0
RAMLS3 size: 0x800 unused: 0x0 max hole: 0x0
RAMLS4 size: 0x800 unused: 0x2e8 max hole: 0x2e8
error #10010: errors encountered during linking; "Six_ph_control_cpu1.out" not built
gmake[1]: *** [Six_ph_control_cpu1.out] Error 1
makefile:160: recipe for target 'all' failed
gmake: *** [all] Error 2
**** Build Finished ****
--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Below is my memory code.
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
BEGIN : origin = 0x000000, length = 0x000002
RAMM0 : origin = 0x000122, length = 0x0002DE
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x001000
RAMGS2 : origin = 0x00E000, length = 0x001000
RAMGS3 : origin = 0x00F000, length = 0x001000
RAMGS4 : origin = 0x010000, length = 0x001000
RAMGS5 : origin = 0x011000, length = 0x001000
RAMGS6 : origin = 0x012000, length = 0x001000
RAMGS7 : origin = 0x013000, length = 0x001000
RAMGS8 : origin = 0x014000, length = 0x001000
RAMGS9 : origin = 0x015000, length = 0x001000
RAMGS10 : origin = 0x016000, length = 0x001000
// RAMGS11 : origin = 0x017000, length = 0x001000
// RAMGS12 : origin = 0x018000, length = 0x001000
// RAMGS13 : origin = 0x019000, length = 0x001000
RAMGS14 : origin = 0x01A000, length = 0x001000
RAMGS15 : origin = 0x01B000, length = 0x001000
CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
}
--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Below is my Section code.
SECTIONS
{
codestart : > BEGIN, PAGE = 0
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
.TI.ramfunc : {} > RAMM0, PAGE = 0
#else
ramfuncs : > RAMM0 PAGE = 0
#endif
#endif
.text : >>RAMM0 | RAMD0 | RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4, PAGE = 0
.cinit : > RAMLS4, PAGE = 0
.pinit : > RAMM0, PAGE = 0
.switch : > RAMM0, PAGE = 0
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.stack : > RAMM1, PAGE = 1
.bss : > RAMLS5, PAGE = 1
.const : > RAMLS5, PAGE = 1
.sysmem : > RAMLS5, PAGE = 1
.data : > RAMLS5, PAGE = 1
Filter_RegsFile : > RAMGS0, PAGE = 1
ramgs0 : > RAMGS0, PAGE = 1
ramgs1 : > RAMGS1, PAGE = 1
.init_array : > RAMGS2, PAGE = 1
motorData : > RAMGS3, PAGE = 1
controlData : > RAMGS3, PAGE = 1
ipcData : > RAMGS4, PAGE = 1
States1 : >> RAMGS5 | RAMGS6, PAGE = 1
States2 : >> RAMGS7 | RAMGS8, PAGE = 1
LUT : >> RAMGS9, PAGE = 1
/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}
GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
How can I increase the memory portion of Page 0?