This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Script exit code: 126 for check_depends.sh during CCS 10.4.0 installation on Linux

Other Parts Discussed in Thread: CC2538, SYSCONFIG

Hello, I am installing CCS 10.4.0 on Linux and am having issues with the installer. I understand 

Exit code: 126 suggests the file is not an executable. Any ideas why check_depends.sh is not generated as an executable?

My laptop configuration: 

Linux kernel: 4.9.0-13-amd64

Linux distribution: Debian GNU/Linux 9 (stretch)

Architecture: x86_64

I've already tried: 

1. Both the single file and on-demand installer from TI website

2. Running after installing the libraries listed here https://software-dl.ti.com/ccs/esd/documents/ccsv10_linux_host_support.html

3. Running after applying 'chmod -R 777' to the setup.run file

4. Running with sudo

5. Checking that username/directories do not spaces

Here is the error message 

I found a log in /tmp/ ccs_install_10.4.0.00006.log, please see the log pasted below.

=========================================
Log started 08/04/2021 at 14:44:43
Preferred installation mode : gtk
Trying to init installer in mode gtk
Mode gtk successfully initialized
[14:44:46] CCS_INFO: Installer timestamp 20210804144446
[14:44:46] Installer arguments
[14:44:46] CCS_INFO: Initialization sets components_download_url to software-dl.ti.com/.../components
[14:44:46] createshortcuts set to true
[14:44:46] CCS_INFO: Temporary folder set to /tmp/ccs_9ed2bcd3-6dca-4f3c-7578-dbc160af4a07
[14:44:46] CCS_INFO: Product families available: PF_MSP430,PF_MSP432,PF_CC2X,PF_CC3X,PF_CC2538,PF_C28,PF_TM4C,PF_HERCULES,PF_SITARA,PF_SITARA_MCU,PF_OMAPL,PF_DAVINCI,PF_OMAP,PF_TDA_DRA,PF_C55,PF_C6000SC,PF_C66AK_KEYSTONE,PF_MMWAVE,PF_C64MC,PF_DIGITAL_POWER,PF_PGA
[14:44:47] CCS_INFO: Components available: ARM_CGT_HELP,C2000_CGT_HELP,C6000_CGT_HELP,CCS_DOC,CCS_LAUNCHER,CCS_UTILS,CGT_DEFAULTLIBS_C2800,CGT_DEFAULTLIBS_C6000_V8P,CGT_DEFAULTLIBS_MSP430,CGT_DEFAULTLIBS_TMS470,CLOUDAGENT,DEV_SUPPORT_AUTOMOTIVE,DEV_SUPPORT_C55XX,DEV_SUPPORT_C6000,DEV_SUPPORT_CC2538,DEV_SUPPORT_CC26XX,DEV_SUPPORT_CC3220,DEV_SUPPORT_CC3230,DEV_SUPPORT_CC32XX,DEV_SUPPORT_CC32XX_COMMON,DEV_SUPPORT_DAVINCI,DEV_SUPPORT_INTEGRA,DEV_SUPPORT_MMWAVE,DEV_SUPPORT_OMAP,DEV_SUPPORT_PGA,DEV_SUPPORT_SHARED,DEV_SUPPORT_SITARA,DEV_SUPPORT_SITARA_MCU,DEV_SUPPORT_UCD31XX,DMED,DS,DS_FLASH,DVT,ECLIPSE,EMU_BH,EMU_C2000,EMU_C2000_FLASH,EMU_HERCULES,EMU_TI,GCC_ARM_COMPILER,GCC_MSP430_COMPILER,IDE,IDE_CHROME,IDE_GC,IDE_TOOLS_COMMON,INSTALLER,JRE,KEYSTONE2,MSP430_BUILD_DEBUG,MSP430_CGT_HELP,MSP430_GCC_SUPPORT,MSP432_BUILD_DEBUG,NODEJS,P2APP,P2TOOLS,SEGGER_J_LINK,SYSCONFIG,TARGETDB_DEF_PROPS,TARGET_CONTENT_CORE,TIREX,TIREX4,TIVA_STELLARIS_DRIVERS,TIVA_TM4C,TIVA_TM4E,TI_ARM_CLANG,USERGUIDE,core
[14:44:47] PFsToBeInstalled:
[14:44:47] CCS_INFO: Components default folder is set to /home/USERNAME/Downloads/components
[14:44:47] CCS_INFO: Components override folder is set to /home/USERNAME/Downloads/components
Executing /tmp/ccs_9ed2bcd3-6dca-4f3c-7578-dbc160af4a07/util/dependency-checker/check_depends.sh
Script exit code: 126

Script output:

Script stderr:
/bin/sh: 1: /tmp/ccs_9ed2bcd3-6dca-4f3c-7578-dbc160af4a07/util/dependency-checker/check_depends.sh: Permission denied

Error running /tmp/ccs_9ed2bcd3-6dca-4f3c-7578-dbc160af4a07/util/dependency-checker/check_depends.sh : /bin/sh: 1: /tmp/ccs_9ed2bcd3-6dca-4f3c-7578-dbc160af4a07/util/dependency-checker/check_depends.sh: Permission denied
[14:44:52] CCS_INFO: In installationAbortedActionList
[14:44:52] Moving logfile /tmp/installbuilder_installer_29845.log to /tmp/ccs_install_10.4.0.00006.log

===============================

Thanks for reading,