Configuration:
Software: a fresh install of CCSv4, NDK 2.20.3.24 and NSP 1.0.0.9
Hardware: LogicPD c6748 EVM.
The target configuration is evmc6748.ccxml from the logicpd bsl.
When trying to run any of the examples in the NSP on C6748 evm, the following error is obtained
C674X_0: File Loader: Data verification failed at address 0xC30CD000 Please verify target memory and memory map.
Error found during data verification.
Ensure the linker command file matches the memory map.
Is that a bug? How are the NSP examples supposed to be run?