This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv10 (under windows) cannot restart after latest update

After responding to a notification that a new update was available, the update was applied and CCSv10 attempted to restart, but the result was the display of two dialogs: (1) a dialog entitled "Setup" with an empty progress bar and NO text, and (2) a dialog entitled "Error" with the text:

    There has been an error.
    Error processing regular expression /(nickname|name)=***unknown variable updatename***

and an "OK" button.

There is no indication as to what file is being processed when the error occurs.

There appears to be no way to use CCSv10 at this point.

  • Hello,

    I've never seen that error before. Was a CCS 10.4.0 incremental update? If so, what version did you upgrade from?

    I assume you get the same error with repeated attempts to launch CCS?

    Thanks

    ki

  • Yes, to the question about getting the same error if I try to start CCSv10 on my own.

    As to the nature of the update, all I can recall is that there was only one item in the list.  I believe it was an update to the compiler tools for MSP430 as opposed to the CCSv10 environment.  The only thing I recall is there was an "8" in the version number, but I cannot recall the full number.  Since I cannot now start up CCS, there is no way for me to query any of the versions.  Alas, this means I cannot tell you what version I was updating from, or to.  On the other hand, what I can say is that I installed the new CCSv10 in place of CCSv6 earlier this month, and the last update I did prior to today was just a couple weeks ago (08/16/21), so one supposes I'd be running a fairly current version of CCSv10 and the MSP430 toolset.

    In the event, if I look in the C:\TI directory tree, I see a folder called "ccs1011".  In that, there is a "ccs" folder and a "xdctools_3_61_02_27_core" directory.  Oddly enough, in the "ccs" folder there is a folder called "install_info" that contains two folders: one called "10.1.1.00004" with today's date and another called "10.2.0.00009" with a date of August 9, 2021 (which sounds like it could have been the last time I did an update).  From the names of the folders, however, they seem "backwards" -- like a 10.2.0 version build was "updated" to a 10.1.1 build (though I can't say for sure since I don't know how TI names these things.  In fact, I just checked the files (v. folders) in that same directory, and the only files that match the date (today's) of the 10.1.1.00004 folder I mentioned have the string "msp432" in them, which suggests that today's update was only for the MSP432 family tools rather than the MSP430 tools.  The two files in question are "com.ti.msp432.build_debug.properties" and "com.ti.msp432.support_files.properties". Both of these seem trivial in the sense that they contain a "Featureid" setting (that matches the file name) and a "Version" (8.2.4 for the "build_debug" file and 8.2.3 for the "support_files" file), but the remaining entries are blank; that is:

    Binary=
    Installdir=
    Tag=

    Meanwhile, there is an "install_logs" folder parallel to the "install_info" folder, and it contains a number of sub-folders.  Somewhat surprisingly, there are FIVE such folders with today's date.  Each of these has a name that matches the timestamp (e.g., "20210826104159", ..., "20210826111708").  ALL FIVE of these folders contain just one file with the same exact name: "ccs_update_10.4.0.00006.log".  I'm going to guess these represent the number of times I've tried to re-start CCS to install the update.  Since the error occurred on the very first try, one supposes the content of the earliest file may be salient; this is:

    Log started 08/26/2021 at 10:41:58
    Preferred installation mode : unattended
    Trying to init installer in mode win32
    Mode win32 successfully initialized
    [10:41:59] CCS_INFO: Installer timestamp 20210826104159
    [10:41:59] Installer arguments --ccs true
    [10:41:59] CCS_INFO: Temporary folder set to C:\Users\Gary\AppData\Local\Temp/ccs_2e7b92e1-d30e-4de1-455d-733361073e4d
    [10:42:01] CCS_INFO: Modified override url to
    [10:42:01] CCS_INFO: Latest installer is C:\ti\ccs1011\ccs\eclipse\downloads\ccs_setup_10.4.0.00006.exe
    [10:42:01] CCS_INFO: PrefsFile: C:/ti/ccs1011/ccs/eclipse/p2/org.eclipse.equinox.p2.engine/profileRegistry/epp.package.cpp.profile/.data/.settings/org.eclipse.equinox.p2.metadata.repository.prefs
    [10:42:02] Moving logfile to C:/ti/ccs1011/ccs/install_logs/20210826104159/ccs_update_10.4.0.00006.log

    If I look in the path mentioned in the "Latest installer" entry of the log file, I can see that there are THREE executables with today's date: ccs_update_10.1.1.00004.exe, ccs_update_10.2.0.00009.exe, ccs_update_10.4.0.00006.exe, and "startupInstaller_6.0.0.202001271514.log".  The content of this final file is:


    Logging on 2020/12/16 15:44:38
    2020-12-16 15:44:38.882: copying ccs_update_10.1.1.00004.exe
    2020-12-16 15:44:38.882: in copyFiles, copying utils to downloads
    2020-12-16 15:44:38.897: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.1.1.00004.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.1.1.00004.exe
    SI_MAIN: higestfile = ccs_update_10.1.1.00004.exe
    SI_MAIN: utilFile = ccs_update_10.1.1.00004.exe
    highest file is not null
    SI_MAIN: Find file to run C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.1.1.00004.exe
    SI_MAIN: exec cmdargs[0] cmd.exe
    SI_MAIN: exec cmdargs[1] /c
    SI_MAIN: exec cmdargs[2] C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.1.1.00004.exe
    SI_MAIN: exec cmdargs[3] --ccs
    SI_MAIN: exec cmdargs[4] true
    SI_MAIN: exit code 0

    Logging on 2021/08/09 10:50:20
    2021-08-09 10:50:20.145: copying ccs_update_10.1.1.00004.exe
    2021-08-09 10:50:20.145: in copyFiles, copying utils to downloads
    2021-08-09 10:50:20.145: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.1.1.00004.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.1.1.00004.exe
    SI_MAIN: higestfile = ccs_update_10.1.1.00004.exe
    SI_MAIN: utilFile = ccs_update_10.1.1.00004.exe
    highest file is not null
    SI_MAIN: Find file to run C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.1.1.00004.exe
    SI_MAIN: exec cmdargs[0] cmd.exe
    SI_MAIN: exec cmdargs[1] /c
    SI_MAIN: exec cmdargs[2] C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.1.1.00004.exe
    SI_MAIN: exec cmdargs[3] --ccs
    SI_MAIN: exec cmdargs[4] true
    SI_MAIN: exit code 0

    Logging on 2021/08/09 14:19:23
    2021-08-09 14:19:24.010: copying ccs_update_10.1.1.00004.exe
    2021-08-09 14:19:24.010: in copyFiles, copying utils to downloads
    2021-08-09 14:19:24.010: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.1.1.00004.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.1.1.00004.exe
    2021-08-09 14:19:24.088: copying ccs_update_10.2.0.00009.exe
    2021-08-09 14:19:24.088: in copyFiles, copying utils to downloads
    2021-08-09 14:19:24.088: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.2.0.00009.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.2.0.00009.exe
    SI_MAIN: higestfile = ccs_update_10.2.0.00009.exe
    SI_MAIN: utilFile = ccs_update_10.2.0.00009.exe
    highest file is not null
    SI_MAIN: Find file to run C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.2.0.00009.exe
    SI_MAIN: exec cmdargs[0] cmd.exe
    SI_MAIN: exec cmdargs[1] /c
    SI_MAIN: exec cmdargs[2] C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.2.0.00009.exe
    SI_MAIN: exec cmdargs[3] --ccs
    SI_MAIN: exec cmdargs[4] true
    SI_MAIN: exit code 0

    Logging on 2021/08/16 11:23:02
    2021-08-16 11:23:02.731: copying ccs_update_10.1.1.00004.exe
    2021-08-16 11:23:02.731: in copyFiles, copying utils to downloads
    2021-08-16 11:23:02.731: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.1.1.00004.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.1.1.00004.exe
    2021-08-16 11:23:02.872: copying ccs_update_10.2.0.00009.exe
    2021-08-16 11:23:02.872: in copyFiles, copying utils to downloads
    2021-08-16 11:23:02.872: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.2.0.00009.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.2.0.00009.exe
    2021-08-16 11:23:02.919: copying ccs_update_10.4.0.00006.exe
    2021-08-16 11:23:02.919: in copyFiles, copying utils to downloads
    2021-08-16 11:23:02.919: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.4.0.00006.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: higestfile = ccs_update_10.4.0.00006.exe
    SI_MAIN: utilFile = ccs_update_10.4.0.00006.exe
    highest file is not null
    SI_MAIN: Find file to run C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: exec cmdargs[0] cmd.exe
    SI_MAIN: exec cmdargs[1] /c
    SI_MAIN: exec cmdargs[2] C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: exec cmdargs[3] --ccs
    SI_MAIN: exec cmdargs[4] true
    SI_MAIN: exit code 0

    Logging on 2021/08/26 10:41:45
    2021-08-26 10:41:45.679: copying ccs_update_10.1.1.00004.exe
    2021-08-26 10:41:45.679: in copyFiles, copying utils to downloads
    2021-08-26 10:41:45.679: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.1.1.00004.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.1.1.00004.exe
    2021-08-26 10:41:46.319: copying ccs_update_10.2.0.00009.exe
    2021-08-26 10:41:46.319: in copyFiles, copying utils to downloads
    2021-08-26 10:41:46.319: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.2.0.00009.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.2.0.00009.exe
    2021-08-26 10:41:46.619: copying ccs_update_10.4.0.00006.exe
    2021-08-26 10:41:46.619: in copyFiles, copying utils to downloads
    2021-08-26 10:41:46.619: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.4.0.00006.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: higestfile = ccs_update_10.4.0.00006.exe
    SI_MAIN: utilFile = ccs_update_10.4.0.00006.exe
    highest file is not null
    SI_MAIN: Find file to run C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: exec cmdargs[0] cmd.exe
    SI_MAIN: exec cmdargs[1] /c
    SI_MAIN: exec cmdargs[2] C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: exec cmdargs[3] --ccs
    SI_MAIN: exec cmdargs[4] true
    SI_MAIN: exit code 0

    Logging on 2021/08/26 10:42:18
    2021-08-26 10:42:18.784: copying ccs_update_10.1.1.00004.exe
    2021-08-26 10:42:18.784: in copyFiles, copying utils to downloads
    2021-08-26 10:42:18.794: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.1.1.00004.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.1.1.00004.exe
    2021-08-26 10:42:18.834: copying ccs_update_10.2.0.00009.exe
    2021-08-26 10:42:18.834: in copyFiles, copying utils to downloads
    2021-08-26 10:42:18.834: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.2.0.00009.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.2.0.00009.exe
    2021-08-26 10:42:18.854: copying ccs_update_10.4.0.00006.exe
    2021-08-26 10:42:18.854: in copyFiles, copying utils to downloads
    2021-08-26 10:42:18.854: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.4.0.00006.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: higestfile = ccs_update_10.4.0.00006.exe
    SI_MAIN: utilFile = ccs_update_10.4.0.00006.exe
    highest file is not null
    SI_MAIN: Find file to run C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: exec cmdargs[0] cmd.exe
    SI_MAIN: exec cmdargs[1] /c
    SI_MAIN: exec cmdargs[2] C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: exec cmdargs[3] --ccs
    SI_MAIN: exec cmdargs[4] true
    SI_MAIN: exit code 0

    Logging on 2021/08/26 10:44:23
    2021-08-26 10:44:23.228: copying ccs_update_10.1.1.00004.exe
    2021-08-26 10:44:23.228: in copyFiles, copying utils to downloads
    2021-08-26 10:44:23.228: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.1.1.00004.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.1.1.00004.exe
    2021-08-26 10:44:23.263: copying ccs_update_10.2.0.00009.exe
    2021-08-26 10:44:23.263: in copyFiles, copying utils to downloads
    2021-08-26 10:44:23.263: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.2.0.00009.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.2.0.00009.exe
    2021-08-26 10:44:23.291: copying ccs_update_10.4.0.00006.exe
    2021-08-26 10:44:23.291: in copyFiles, copying utils to downloads
    2021-08-26 10:44:23.291: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.4.0.00006.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: higestfile = ccs_update_10.4.0.00006.exe
    SI_MAIN: utilFile = ccs_update_10.4.0.00006.exe
    highest file is not null
    SI_MAIN: Find file to run C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: exec cmdargs[0] cmd.exe
    SI_MAIN: exec cmdargs[1] /c
    SI_MAIN: exec cmdargs[2] C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: exec cmdargs[3] --ccs
    SI_MAIN: exec cmdargs[4] true
    SI_MAIN: exit code 0

    Logging on 2021/08/26 11:04:04
    2021-08-26 11:04:04.246: copying ccs_update_10.1.1.00004.exe
    2021-08-26 11:04:04.248: in copyFiles, copying utils to downloads
    2021-08-26 11:04:04.248: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.1.1.00004.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.1.1.00004.exe
    2021-08-26 11:04:04.306: copying ccs_update_10.2.0.00009.exe
    2021-08-26 11:04:04.306: in copyFiles, copying utils to downloads
    2021-08-26 11:04:04.308: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.2.0.00009.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.2.0.00009.exe
    2021-08-26 11:04:04.338: copying ccs_update_10.4.0.00006.exe
    2021-08-26 11:04:04.338: in copyFiles, copying utils to downloads
    2021-08-26 11:04:04.338: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.4.0.00006.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: higestfile = ccs_update_10.4.0.00006.exe
    SI_MAIN: utilFile = ccs_update_10.4.0.00006.exe
    highest file is not null
    SI_MAIN: Find file to run C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: exec cmdargs[0] cmd.exe
    SI_MAIN: exec cmdargs[1] /c
    SI_MAIN: exec cmdargs[2] C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: exec cmdargs[3] --ccs
    SI_MAIN: exec cmdargs[4] true
    SI_MAIN: exit code 0

    Logging on 2021/08/26 11:16:56
    2021-08-26 11:16:56.873: copying ccs_update_10.1.1.00004.exe
    2021-08-26 11:16:56.873: in copyFiles, copying utils to downloads
    2021-08-26 11:16:56.873: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.1.1.00004.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.1.1.00004.exe
    2021-08-26 11:16:56.903: copying ccs_update_10.2.0.00009.exe
    2021-08-26 11:16:56.903: in copyFiles, copying utils to downloads
    2021-08-26 11:16:56.903: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.2.0.00009.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.2.0.00009.exe
    2021-08-26 11:16:56.933: copying ccs_update_10.4.0.00006.exe
    2021-08-26 11:16:56.933: in copyFiles, copying utils to downloads
    2021-08-26 11:16:56.933: copyFile: C:\ti\ccs1011\ccs\eclipse\utils\ccs_update_10.4.0.00006.exe to C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: higestfile = ccs_update_10.4.0.00006.exe
    SI_MAIN: utilFile = ccs_update_10.4.0.00006.exe
    highest file is not null
    SI_MAIN: Find file to run C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: exec cmdargs[0] cmd.exe
    SI_MAIN: exec cmdargs[1] /c
    SI_MAIN: exec cmdargs[2] C:\ti\ccs1011\ccs\eclipse\downloads\ccs_update_10.4.0.00006.exe
    SI_MAIN: exec cmdargs[3] --ccs
    SI_MAIN: exec cmdargs[4] true
    SI_MAIN: exit code 0

    Nothing in any of this seems obviously problematic, so I'm not sure it's useful at all, but if there is anything else you may need to see to help diagnose the failure, I can try to supply it.  I really need to get back to working order, as this really could not have happened at a more critical time.

  • It looks like an incremental update attempt to CCS 10.4.0. I will need to pull in our installer/update expert so see what happened.

    I really need to get back to working order, as this really could not have happened at a more critical time.

    Given that this is a critical time, you are likely better off just doing a full CCS 10.4.0 installation from the the official 10.4.0 installer:

    https://dev.ti.com/tirex/explore/node?node=ABWY3rK-TxFNJWhggQeVug__FUz-xrs__LATEST

    Thanks

    ki