This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv5 Data Formatting in Expressions Window



Do we have plans (e.g. in CCS 5.1) to add back the capability to choose the display type on a line by line basis?  I see from the CCSv5 Changes page that this was something we "lost" when moving to stock eclipse.  I was curious if this is one of the things we'll get back (like multiple instances of windows) in the Indigo release.

  • We have made open source contributions to enable this. CCS v5.1 M3 (available on the web) has this support. It also has support for being able to open multiple basic debug views (e.g. disassembly, memory). 

     

    martin