This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Where are my files?



I'm working with CCSv4 and the TI 2808 Docking Station.

I created all my code using the existing test code for guidance.  I think I have a "project" called VGC which works fine on my machine.  I copy the complete workspace directory to another machine downstairs and install CCSv4 on the downstairs machine.  I import my projects and my VGC project doesn't show up.  There's a folder for it but the only thing in the folder is a 4k .project file.  The example code folders all have a .project file, .cdtbuild file, a .cdtproject file, a macros.ini file, and an Example_280xBLAH.c file.  When I pull in any other projects I was trying to create (that never worked) I get an error claiming the auto make file is missing.  I can't find my code for the VGC project at all.

How do I move my data from one machine to the other?  Or it seems the better question is, why don't I have the project in my workspace like I thought I had?  Is my data being stored elsewhere?  Have I created a bad project?  I think I remember not being able to successfully create a new project so I renamed an existing project to VGC and changed everything I could find to VGC.

The directions for creating a project are very simple to follow except it doesn't actually create a project that sees all the headers and .c code that is required (ADC, CAN, ePWM, etc.).  I think I remember other things missing.  How do I create projects that are portable and see all the .h and .c files created for 2808 and has all the support command files, etc. that are required for a project? 

Thanks,

Rick