Processors: 6457 (irrelevant because we don't connect yet).
Spectrum Digital Device 1 : XDS560 v2 travellers USB
Spectrum Digital Device 2 : XDS560 v2 travellers USB
Target Configuration:
Add one device, set I/O Port number to 0
Add another device to same target configuration, I/O Port Number 1.
Steps to crash:
1. After setting up the configuration above, in the target configuration window, hit "Connect" (I think this is the wording) to connect to the emulator(s)?
2. Code Composer Studio 5.1 IDE disapears
Note: Same behavior happens in Code Composer 6.
We really can't move to a newer version at this time.
Any suggestions?