Other Parts Discussed in Thread: TMS320F280023C, LAUNCHXL-F280025C, SYSCONFIG
Hi
We have created a target where we routed one of the devices uart out into the jtag connector.
The target is based on TMS32F28003c
I use a XDS200 from Sprectrum Digital.
I use the latest CCS
I have managed to setup the debugger so that I get messages sendt from my target into a serial terminal.
But only as long as there is an active debugging session.
When i flash SW into the target, I see the first messages popping up on the serial terminal. but as soon as the debug session (opened by the flash routine in CCS) closes down terminal is silent.
If I start a debug session, and let the processor free run, the messages keeps popping up in the serial terminal. until I send the debug session, then it turns silent again.
I tried different setting for the debugger with no luck so far.
Below you my target config and the output from test connection.
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="Texas Instruments XDS2xx USB Debug Probe_0">
<instance XML_version="1.2" desc="Texas Instruments XDS2xx USB Debug Probe_0" href="connections/TIXDS2XXUSB_Connection.xml" id="Texas Instruments XDS2xx USB Debug Probe_0" xml="TIXDS2XXUSB_Connection.xml" xmlpath="connections"/>
<connection XML_version="1.2" id="Texas Instruments XDS2xx USB Debug Probe_0">
<instance XML_version="1.2" href="drivers/tixds560icepick_c.xml" id="drivers" xml="tixds560icepick_c.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds560c28x.xml" id="drivers" xml="tixds560c28x.xml" xmlpath="drivers"/>
<property Type="choicelist" Value="2" id="The cJTAG / SWD Features">
<choice Name="cJTAG (1149.7) 2-pin advanced modes" value="enable">
<property Type="choicelist" Value="0" id="The Target Scan Format"/>
<property Type="choicelist" Value="1" id="XDS200 User Port"/>
</choice>
</property>
<property Type="choicelist" Value="1" id="The JTAG TCLK Frequency (MHz)">
<choice Name="Adaptive with user specified limit" value="ADAPTIVE">
<property Type="stringfield" Value="20.0MHz" id="-- Enter a value from 0.5MHz to 20.0MHz"/>
</choice>
</property>
<property Type="choicelist" Value="0" id="The JTAG Signals Isolation Upon Disconnect"/>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="TMS320F280023C_0" href="devices/f280023c.xml" id="TMS320F280023C_0" xml="f280023c.xml" xmlpath="devices"/>
</platform>
</connection>
</configuration>
</configurations>
[Start: Texas Instruments XDS2xx USB Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\u246135\AppData\Local\TEXASI~1\
CCS\ccs1010\2\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
The library build date was 'Jun 25 2021'.
The library build time was '16:23:59'.
The library package version is '9.4.0.00129'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '13' (0x0000000d).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
This emulator does not create a reset log-file.
-----[Perform the Integrity scan-test on the JTAG IR]------------------------
This test will use blocks of 64 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG IR Integrity scan-test has succeeded.
-----[Perform the Integrity scan-test on the JTAG DR]------------------------
This test will use blocks of 64 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG DR Integrity scan-test has succeeded.
[End: Texas Instruments XDS2xx USB Debug Probe_0]