This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CODECOMPOSER: Project Wizard doesn't show examples for MSP-EXP432P401R

Part Number: CODECOMPOSER

I recently downloaded CCS11 and started working on a project that uses MSP-EXP432P401R Launchpad REV 2.0.  The device is recognized by CCS however, even though I downloaded and manually installed SimpleLink MSP432P4 SDK 3.40.01.02 and added it to Window -> Preferences -> Code Composer Studio -> Products, when I click on Getting Started -> Browse and Import Examples it does not show me the examples from this SDK.  Is there something else I need to do to make this board available to CCS11? 

I have also tried using Resource Explorer however it only has Software for SimpleLink MSP432E4 SDK 4.20.00.12 and I can find no way to add as new "Package" to the Resource Explorer.  I would think the Package Manager would allow for importing of an SDK but it doesn't seem to have a "New" or "Add" button.  Is there a way to add this board/SDK to the Resource Explorer?