I am currently trying to migrate from CCS v3.3 to CCS v4.x, using the Blackhawk USB560 and OMAP 2430 configuration. I believe I have just about everything working, but I have a few questions about some details:
1) In my configuration, I have the connection, a router n(IcePick_B_0), and 3 subpaths under that labeled: arm w/ARM11 processor, etb w/BYPASSP_ETB processor, and dsp w/C64xx_0 processor. When I launch the configuration I right-click on the ARM11_0 subpath I created to connect to my target, OMAP2430 processor. Do I need the other two?
2) In my v3.3 configuration, a C6400Plus CPU is setup under the dsp subpath and points to the C6400plus driver. In v4.x, I don't know how to get the C6400Plus CPU or how to "link" to the C6400plus driver, which is why I chose C64xx_0. If it is not need from question 1 above, then I have no concern.
3) Before loading memory, I use two files using the "Load Program" option: x-loader.out and u-boot.out. Using a u-boot.out file, in v3.3 everything seems to behave normally when I "Load Program". However, in v4.x, I see a bunch of nand bad block errors and I also see a line in the terminal window after the programming of u-boot that says something like, "bug found in u-boot on line c.248". I can still complete the process of loading FW through the "Load Memory" option after this step, but I don't see this sort of behavior with v3.3 and didn't know if I had corrupted u-boot files or needed new ones or what.
Thanks for your help.