Part Number: CODECOMPOSER
Other Parts Discussed in Thread: TMS320C28345, SYSCONFIG
Hello,
I am attempting to update a C2000 project (TMS320C28345) from CCS4 and DSP/BIOS to CCS10 and SYS/BIOS.
I used the "Migrating a DSP/BIOS 5 Application to SYS/BIOS 6" as reference.
Used the ti.bios.conversion tool to create a new .cfg file and created a new project in CCS10 with it.
After copying the source from the old project in and fixing the include paths, I am getting 400+ errors of the same type:
#20 identifier "Arg" is undefined
"BUF_alloc"
"DATALOG_ISR"
Ect.
Many are from the /DSP2834x_common/ files.
Using the following tool versions:
CCS Version: 10.4.0.00006
TI C2000 v20.2.5.LTS
SYS/BIOS 6.83.0.18
SysConfig 1.9.0
XDCtools 3.62.1.15_core
Any suggestions on what is causing this would be appreciated. Thank you.