Part Number: CODECOMPOSER
Hi team,
Take TI's picture as an example, PORT1 is the main function with TA1 and TA2 subfunctions.

For Inclusive Size:
| PORT1 | 32 |
| TA1 | 8 |
| TA2 | 8 |
Issue: If TA1 and TA2 are in PORT1 as the structure: if(){TA1}else{TA2}, regardless of how much PORT1 is used, the program will only feed into TA1 and TA2 at a time, and the PORT1 will not have any effect, even 100%. Is that right?
Could you help check this case? Thanks.
Best Regards,
Cherry