Other Parts Discussed in Thread: PMP21529, UCD3138, UCD3138A
Hi Ki,
Per your comments, I tried the ccs 6.2 offline installer and it's successfully installed. However, I run into the build-up error with the log below. It looks .obj file is not generated. Could you advise how to solve it?
**** Clean-only build of configuration Debug for project PMP21529 ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k clean
DEL /F "PMP21529.out" "PMP21529.hex"
DEL /F "clear_program_flash.obj" "constants.obj" "cyclone_global_variables_defs.obj" "device_id.obj" "flash.obj" "init_adc12.obj" "init_bat_charge_loop.obj" "init_bus_backup_loop.obj" "init_dpwm.obj" "init_miscellaneous.obj" "init_protection.obj" "interrupts.obj" "main.obj" "pmbus.obj" "pmbus_coefficients.obj" "pmbus_handler.obj" "pmbus_manuf_info_commands.obj" "pmbus_manuf_specific_commands.obj" "pmbus_tools.obj" "software_interrupt_wrapper.obj" "standard_interrupt.obj" "zero_out_integrity_word.obj"
Could Not Find C:\Users\a0486368\Documents\FAE_SSNW\HERE!---------------------------------------------------Review Format\HVC\UCD3138A\FirmwareCode_ReferenceDesigns\PMP21529_4SWBuckBoostBIDIConverter\PMP21529Firmware-1.0\PMP21529 package\UCD3138_PMP21529\Debug\PMP21529.out
Could Not Find C:\Users\a0486368\Documents\FAE_SSNW\HERE!---------------------------------------------------Review Format\HVC\UCD3138A\FirmwareCode_ReferenceDesigns\PMP21529_4SWBuckBoostBIDIConverter\PMP21529Firmware-1.0\PMP21529 package\UCD3138_PMP21529\Debug\clear_program_flash.obj
'Finished clean'
' '
**** Build Finished ****
**** Build of configuration Debug for project PMP21529 ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building target: PMP21529.out'
'Invoking: ARM Linker'
"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 -g --preproc_with_compile --preproc_with_comment --diag_warning=225 --display_error_number -z -m"C:/Users/a0486368/Documents/FAE_SSNW/HERE!---------------------------------------------------Review Format/HVC/UCD3138A/FirmwareCode_ReferenceDesigns/PMP21529_4SWBuckBoostBIDIConverter/PMP21529Firmware-1.0/PMP21529 package/UCD3138_PMP21529/PMP21529.map" --heap_size=10 --stack_size=200 -i"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/lib" -i"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/include" --reread_libs --display_error_number --warn_sections --xml_link_info="PMP21529_linkInfo.xml" --rom_model -o "PMP21529.out" "./clear_program_flash.obj" "./constants.obj" "./cyclone_global_variables_defs.obj" "./device_id.obj" "./flash.obj" "./init_adc12.obj" "./init_bat_charge_loop.obj" "./init_bus_backup_loop.obj" "./init_dpwm.obj" "./init_miscellaneous.obj" "./init_protection.obj" "./interrupts.obj" "./main.obj" "./pmbus.obj" "./pmbus_coefficients.obj" "./pmbus_handler.obj" "./pmbus_manuf_info_commands.obj" "./pmbus_manuf_specific_commands.obj" "./pmbus_tools.obj" "./software_interrupt_wrapper.obj" "./standard_interrupt.obj" "./zero_out_integrity_word.obj" -l"C:/Users/a0486368/Documents/FAE_SSNW/HERE!---------------------------------------------------Review Format/HVC/UCD3138A/FirmwareCode_ReferenceDesigns/PMP21529_4SWBuckBoostBIDIConverter/PMP21529Firmware-1.0/PMP21529 package/Linker Files/cyclone.cmd" -l"C:/Users/a0486368/Documents/FAE_SSNW/HERE!---------------------------------------------------Review Format/HVC/UCD3138A/FirmwareCode_ReferenceDesigns/PMP21529_4SWBuckBoostBIDIConverter/PMP21529Firmware-1.0/PMP21529 package/Linker Files/cyclone_headers.cmd" -llibc.a
<Linking>
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 19: error #10008-D:
cannot find file "./clear_program_flash.obj"
>> Compilation failure
makefile:162: recipe for target 'PMP21529.out' failed
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 20: error #10008-D:
cannot find file "./constants.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 21: error #10008-D:
cannot find file "./cyclone_global_variables_defs.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 22: error #10008-D:
cannot find file "./device_id.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 23: error #10008-D:
cannot find file "./flash.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 24: error #10008-D:
cannot find file "./init_adc12.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 25: error #10008-D:
cannot find file "./init_bat_charge_loop.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 26: error #10008-D:
cannot find file "./init_bus_backup_loop.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 27: error #10008-D:
cannot find file "./init_dpwm.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 28: error #10008-D:
cannot find file "./init_miscellaneous.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 29: error #10008-D:
cannot find file "./init_protection.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 30: error #10008-D:
cannot find file "./interrupts.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 31: error #10008-D:
cannot find file "./main.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 32: error #10008-D:
cannot find file "./pmbus.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 33: error #10008-D:
cannot find file "./pmbus_coefficients.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 34: error #10008-D:
cannot find file "./pmbus_handler.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 35: error #10008-D:
cannot find file "./pmbus_manuf_info_commands.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 36: error #10008-D:
cannot find file "./pmbus_manuf_specific_commands.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 37: error #10008-D:
cannot find file "./pmbus_tools.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 38: error #10008-D:
cannot find file "./software_interrupt_wrapper.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 39: error #10008-D:
cannot find file "./standard_interrupt.obj"
"C:\\Users\\a0486368\\AppData\\Local\\Temp\\290923", line 40: error #10008-D:
cannot find file "./zero_out_integrity_word.obj"
warning #10211-D: cannot resolve archive
C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5/lib/libc.a to a compatible
library, as no input files have been encountered
fatal error #10009: no input files
gmake: *** [PMP21529.out] Error 1
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
When it comes to reason why I need the old version, please kindly check this thread. I found that a firmware code was not built up in ccs v10. Could you also help to build the code in ccs v10?