This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to use resource explorer inside CCS 11

Hello,

I installed CCS v11.0.0.00012 on my pc, I am unable to acces projects using the resource explorer. Whenever I try to import a project into the ide I get this error shown in the image.

These are  the logs that i got when I clicked on details.

t: Could not get agent, make sure to check if the agent is installed before calling this component at C (dev.ti.com/.../bundle.js:14:95833) at g (dev.ti.com/.../bundle.js:14:92489) at l (dev.ti.com/.../bundle.js:21:103569) at dev.ti.com/.../bundle.js:21:97369 at sa (dev.ti.com/.../bundle.js:78:59331) at Ha (dev.ti.com/.../bundle.js:78:66684) at jc (dev.ti.com/.../bundle.js:78:106601) at ml (dev.ti.com/.../bundle.js:78:90017) at dl (dev.ti.com/.../bundle.js:78:89942) at il (dev.ti.com/.../bundle.js:78:87290)
in ForwardRef in div in ForwardRef in div in ForwardRef in ForwardRef in div in t in ForwardRef in _e in div in ForwardRef in ForwardRef in ForwardRef in ForwardRef in div in ForwardRef in div in div in ForwardRef in ForwardRef in ForwardRef in ForwardRef in a in ForwardRef in ForwardRef in ForwardRef in td in ForwardRef in ForwardRef in tr in ForwardRef in ForwardRef in ForwardRef in t in tbody in ForwardRef in ForwardRef in table in ForwardRef in ForwardRef in t in ForwardRef in t in div in div in ForwardRef in ForwardRef in div in ForwardRef in ForwardRef in div in t in ForwardRef in ForwardRef in ForwardRef in ForwardRef in Unknown in ForwardRef in b in r in div in div in ForwardRef in T in t in t in t in t in Unknown in t in Unknown

I have installed Cloud agent on the pc.