This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS11 in ubuntu

Genius 9880 points

Hi,

Customer encountering problem when using the CCS 11, please see details below.

"I've got a problem to use the ccs11 to connect TI ICEV1 board based on the ubuntu 20.04 LTS.

part of error message shows :The value is '-604' (0xfffffda4).
The title is 'SC_ERR_LIB_ANY_LOAD'.

The explanation is:
A required dynamic library could not be installed.
The attempt to load or install the library failed.

All same setting including hardware and software is workable based on the window platform, but it is not workable on Ubuntu platform.

"

Best Regards,
Maynard