I got the following error dialog when I tried to install CCS 5.1.0M3.1:

I don't understand why I got that error. The new installation is located in a unique folder (C:\Program Files\Texas Instruments\ccsv5.1.0M3.1\). After clicking OK the installation continued. It seemed like things installed ok. However, now when I try to setup a target configuration I do not have any Blackhawk drivers:

Are these two things related?
Brad