Hi Team,
Good day.
We would like to ask assistance with the linker problem raised by client a follows:
"I am getting linker errors on the function UARTStdioConfig. This function belongs to the file utils/uartstdio.h. This directory of this file has been added to the project path and is also in the includes folder in the project explorer.
The exact error: Description Resource Path Location Type
unresolved symbol UARTStdioConfig, first referenced in ./main.obj lab2 C/C++ Problem
I am just trying to print out to stdio using UART. This is a compilation error, not an error with the device itself though.
These top file contains the error in the bottom right as well as showing that the file should be properly linked in the left and middle. The bottom file shows my compilations options."
Refer to the snapshot shared below.
Thank you for your support.
Regards,
Archie A.