This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UniFlash : [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations

Other Parts Discussed in Thread: UNIFLASH

Flashing F2837x controlCARD with UniFlash 7.0.0 is successful but while flashing CPU2 I always get  "Error setting the GSxMSEL..." Log below.

I would like my end users not to see any red errors unless there really is a problem.

What is the cause and workaround please?

Thank you very much.

===================================================================

[21/01/2022 09:58:58] [INFO] C28xx_CPU1: GEL Output: Memory Map Initialization Complete
[21/01/2022 09:58:59] [INFO] C28xx_CPU1: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed.
[21/01/2022 09:58:59] [INFO] C28xx_CPU2: GEL Output: Memory Map Initialization Complete
[21/01/2022 09:58:59] [INFO] C28xx_CPU2: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed.
[21/01/2022 10:00:10] [SUCCESS] Program Load completed successfully.
[21/01/2022 10:00:14] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:16] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:16] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:16] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:16] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:16] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:16] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:16] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:17] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:17] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:17] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:17] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:17] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:17] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:17] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:22] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:23] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:24] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:25] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:26] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:27] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:28] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:29] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:30] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:31] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:36] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:37] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:40] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:41] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:42] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:43] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:45] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:46] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:47] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:48] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:50] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:51] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:52] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:53] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:54] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:55] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:56] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:57] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:58] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:00:59] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:00] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:01] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:02] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:03] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:04] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:05] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:06] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:07] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:08] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:09] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:10] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:11] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:12] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:13] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:14] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:15] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:16] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:17] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:17] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:18] [ERROR] C28xx_CPU2: Error setting the GSxMSEL register for Flash operations
[21/01/2022 10:01:24] [SUCCESS] Program Load completed successfully.