This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP 28335 periodic function manager is missing?

Moving for earlier version of the complier to TI 18.1 with cfg file for sys/bios I've noticed that PRD is no longer present underneath clock (TCF). has it been replace by ePWM or ...? looking to create a couple periodic individual timer to timer out if the elapse time is hit. For instance, SCI RX_ISR receive data and then stop for 4 char cycle call a function to process the char that are in. the ISR would reset the timer as char are received.

CCS7.4

SYS/BIOS 6.75