Other Parts Discussed in Thread: C2000WARE
Hi
I'm new to this Texas device and CCS, and I have problem to load code for debug.
I'm tring to run some code on CPU1 and CPU2 using GSRAM area for debug.
CPU0 code is mapped on GS0 and GS1, while CPU2 code is mapped on GS2 and GS3; map
files shown a correct mapping of my code.
Now, when I try to load my code for debug, CPU1 load is ok while I get a load error when CCS load the code section for CPU2 (verify error at address 0xE000).
I noticed that when I'm focused on CPU1 I can read and write each memory location (LS ram , GS ram, etc) in memory browser, while when
I'm focused on CPU2 all memory region are shown as 0 and I cannot write nothing. Moreover the value writed in memory browser on GS RAM from CPU1 are not
visible from CPU2.
I have 2 gel file and each file initialize the memory map in order to access each memory region.
My system is:
Windows10, CCS 8.3.1 and Blackhawk USB 560M
What's wrong in my application? Do I need to do something to enable the second CPU?
Thanks for help