I am having a problem with CCSV4.2.3.I am trying to follow the getting
started with CCS guide. I have installed the license file as I
understand. However, when I try to run the Debugger, I get a message
to load the license file. If I reload the file at that point, I then
get an error indicating that no feature exists. It indicates that the
feature is CCS_CONNECT_ALL and that the FLEXNet error number is
-5.357.
I am using XDS510 USB emulator with TMS320DM6467 Board .
I tried these two link also
http://processors.wiki.ti.com/index.php?title=Activating_CCS
http://processors.wiki.ti.com/index.php/GSG:CCSv4_Running_for_the_first_time