This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS ROV Opening Blank



Hello,

When I try and debug and open the Realtime Object Viewer (ROV) the window opens blank, and does not pull up a "Connect Target" window like it should. Do you know how I can get around this issue so that I can properly use the ROV tool? Thanks.

  • Are you using TI-RTOS?

  • HI James,

    Please provide the below information:

    -CCS version

    -Target/device being used

    -SYS/BIOS version being used

    -XDCtools version being used

    -Host OS version

    Thanks

    ki

  • Kier,

    Yes, I am using TI-RTOS

    Ki,

    - CCS v10.4.0.00006

    - CC2652R1F using XDS200 debugger

    - I am using TI-RTOS

    - XDCtools v3.62.00.08

    - By "Host OS Version" I am not sure what you mean. I am using PC with Windows 10 Enterprise

  • Thanks. There should be no issue with those version. I tried it out in my environment and ROV worked fine.

    What version of TI-RTOS / SYS/BIOS / SDK are you using?

    Can you try cleaning your workspace?

    https://software-dl.ti.com/ccs/esd/documents/users_guide/ccs_troubleshooting.html#clean-the-workspace-or-try-using-a-new-one

    Thanks

    ki

  • Sorry if this is obvious but I get similar blank ROV window if I have inadvertently selected the core group instead of an individual processor in the top left pane.

  • Which "top left pane" are you refferring to? Could you please provide a screenshot?

  • Ki,

    No problem. I tried cleaning my workspace (deleting the .metadata folder and then importing old preferences) and the same issue arises.

    Below are some of the versions of TI products that I am using. I think that I told you the wrong version of XDCtools in the comment earlier, that was my bad. I believe this SimpleLink SDK uses the latest version of TI-RTOS but not sure.

  • I mean the Debug pane. If I select Group 1 and launch ROV, I get a blank window. But if I select CPU1, ROV launches. However, you may not have a multicore processor/project in which case this is irrelevant.

  • Ah I see. I am only selecting one processor for this instead of the entire group so that is not the problem. This was a good theory though.

  • Can you provide the Eclipse error log found in:

    <WORKSPACE FOLDER>/.metadata/.log

  • !SESSION 2022-04-05 08:42:10.974 -----------------------------------------------
    eclipse.buildId=4.14.0.I20191210-0610
    java.version=1.8.0_144
    java.vendor=Oracle Corporation
    BootLoader constants: OS=win32, ARCH=x86_64, WS=win32, NL=en_US
    Framework arguments:  -product com.ti.ccstudio.branding.product
    Command-line arguments:  -os win32 -ws win32 -arch x86_64 -product com.ti.ccstudio.branding.product
    
    This is a continuation of log file C:\Repo\.metadata\.bak_0.log
    Created Time: 2022-04-05 14:05:49.423
    
    !ENTRY com.ti.ccstudio.debug 1 0 2022-04-05 14:05:49.423
    !MESSAGE DS_ERROR: IcePick_C: Power Failure on Target CPU 
    
    
    !ENTRY com.ti.ccstudio.debug 1 0 2022-04-05 14:05:49.696
    !MESSAGE DS_ERROR: Cortex_M4_0: Failed to remove the debug state from the target before disconnecting.  There may still be breakpoint op-codes embedded in program memory.  It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
    
    
    !ENTRY org.eclipse.cdt.managedbuilder.core 4 0 2022-04-05 14:46:18.779
    !MESSAGE failed to remove resources
    !SUBENTRY 1 org.eclipse.cdt.managedbuilder.core 4 0 2022-04-05 14:46:18.779
    !MESSAGE /Raymond_BT_IO_application/Release/Raymond_BT_IO_application.out
    !STACK 1
    org.eclipse.core.internal.resources.ResourceException: Problems encountered while deleting resources.
    	at org.eclipse.core.internal.resources.Resource.delete(Resource.java:770)
    	at org.eclipse.core.internal.resources.Resource.delete(Resource.java:727)
    	at com.ti.ccstudio.project.core.internal.build.temp.BuildDescriptionManager.cleanGeneratedRebuildResources(BuildDescriptionManager.java:265)
    	at com.ti.ccstudio.project.core.internal.build.CCSMakefileGenerator.generateMakefiles(CCSMakefileGenerator.java:318)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.performMakefileGeneration(CommonBuilder.java:1010)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.performPrebuildGeneration(CommonBuilder.java:872)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:752)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:515)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:461)
    	at org.eclipse.core.internal.events.BuildManager$2.run(BuildManager.java:833)
    	at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:220)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:263)
    	at org.eclipse.core.internal.events.BuildManager$1.run(BuildManager.java:316)
    	at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:319)
    	at org.eclipse.core.internal.events.BuildManager.basicBuildLoop(BuildManager.java:371)
    	at org.eclipse.core.internal.events.BuildManager.build(BuildManager.java:392)
    	at org.eclipse.core.internal.resources.Workspace.buildInternal(Workspace.java:515)
    	at org.eclipse.core.internal.resources.Workspace.build(Workspace.java:412)
    	at com.ti.ccstudio.project.core.services.ProjectBuilder.internalBuildProjects(ProjectBuilder.java:394)
    	at com.ti.ccstudio.project.core.services.ProjectBuilder.buildProjects(ProjectBuilder.java:283)
    	at com.ti.ccstudio.debug.launch.CCSLaunchDelegate.buildForLaunch(CCSLaunchDelegate.java:444)
    	at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:834)
    	at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:719)
    	at org.eclipse.debug.internal.ui.DebugUIPlugin.buildAndLaunch(DebugUIPlugin.java:1017)
    	at org.eclipse.debug.internal.ui.DebugUIPlugin$2.run(DebugUIPlugin.java:1220)
    	at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)
    Contains: Could not delete 'C:\Repo\Raymond_BT_IO_application\Release\Raymond_BT_IO_application.out'.
    org.eclipse.core.runtime.CoreException: Problems encountered while deleting files.
    	at org.eclipse.core.internal.filesystem.local.LocalFile.delete(LocalFile.java:142)
    	at org.eclipse.core.internal.resources.ResourceTree.internalDeleteFile(ResourceTree.java:313)
    	at org.eclipse.core.internal.resources.ResourceTree.standardDeleteFile(ResourceTree.java:799)
    	at org.eclipse.core.internal.resources.Resource.unprotectedDelete(Resource.java:1779)
    	at org.eclipse.core.internal.resources.Resource.delete(Resource.java:757)
    	at org.eclipse.core.internal.resources.Resource.delete(Resource.java:727)
    	at com.ti.ccstudio.project.core.internal.build.temp.BuildDescriptionManager.cleanGeneratedRebuildResources(BuildDescriptionManager.java:265)
    	at com.ti.ccstudio.project.core.internal.build.CCSMakefileGenerator.generateMakefiles(CCSMakefileGenerator.java:318)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.performMakefileGeneration(CommonBuilder.java:1010)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.performPrebuildGeneration(CommonBuilder.java:872)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:752)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:515)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:461)
    	at org.eclipse.core.internal.events.BuildManager$2.run(BuildManager.java:833)
    	at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:220)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:263)
    	at org.eclipse.core.internal.events.BuildManager$1.run(BuildManager.java:316)
    	at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:319)
    	at org.eclipse.core.internal.events.BuildManager.basicBuildLoop(BuildManager.java:371)
    	at org.eclipse.core.internal.events.BuildManager.build(BuildManager.java:392)
    	at org.eclipse.core.internal.resources.Workspace.buildInternal(Workspace.java:515)
    	at org.eclipse.core.internal.resources.Workspace.build(Workspace.java:412)
    	at com.ti.ccstudio.project.core.services.ProjectBuilder.internalBuildProjects(ProjectBuilder.java:394)
    	at com.ti.ccstudio.project.core.services.ProjectBuilder.buildProjects(ProjectBuilder.java:283)
    	at com.ti.ccstudio.debug.launch.CCSLaunchDelegate.buildForLaunch(CCSLaunchDelegate.java:444)
    	at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:834)
    	at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:719)
    	at org.eclipse.debug.internal.ui.DebugUIPlugin.buildAndLaunch(DebugUIPlugin.java:1017)
    	at org.eclipse.debug.internal.ui.DebugUIPlugin$2.run(DebugUIPlugin.java:1220)
    	at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)
    Contains: Could not delete: C:\Repo\Raymond_BT_IO_application\Release\Raymond_BT_IO_application.out.
    java.nio.file.FileSystemException: C:\Repo\Raymond_BT_IO_application\Release\Raymond_BT_IO_application.out: The process cannot access the file because it is being used by another process.
    
    	at sun.nio.fs.WindowsException.translateToIOException(Unknown Source)
    	at sun.nio.fs.WindowsException.rethrowAsIOException(Unknown Source)
    	at sun.nio.fs.WindowsException.rethrowAsIOException(Unknown Source)
    	at sun.nio.fs.WindowsFileSystemProvider.implDelete(Unknown Source)
    	at sun.nio.fs.AbstractFileSystemProvider.deleteIfExists(Unknown Source)
    	at java.nio.file.Files.deleteIfExists(Unknown Source)
    	at org.eclipse.core.internal.filesystem.local.LocalFile.internalDelete(LocalFile.java:223)
    	at org.eclipse.core.internal.filesystem.local.LocalFile.delete(LocalFile.java:140)
    	at org.eclipse.core.internal.resources.ResourceTree.internalDeleteFile(ResourceTree.java:313)
    	at org.eclipse.core.internal.resources.ResourceTree.standardDeleteFile(ResourceTree.java:799)
    	at org.eclipse.core.internal.resources.Resource.unprotectedDelete(Resource.java:1779)
    	at org.eclipse.core.internal.resources.Resource.delete(Resource.java:757)
    	at org.eclipse.core.internal.resources.Resource.delete(Resource.java:727)
    	at com.ti.ccstudio.project.core.internal.build.temp.BuildDescriptionManager.cleanGeneratedRebuildResources(BuildDescriptionManager.java:265)
    	at com.ti.ccstudio.project.core.internal.build.CCSMakefileGenerator.generateMakefiles(CCSMakefileGenerator.java:318)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.performMakefileGeneration(CommonBuilder.java:1010)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.performPrebuildGeneration(CommonBuilder.java:872)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:752)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:515)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:461)
    	at org.eclipse.core.internal.events.BuildManager$2.run(BuildManager.java:833)
    	at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:220)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:263)
    	at org.eclipse.core.internal.events.BuildManager$1.run(BuildManager.java:316)
    	at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:319)
    	at org.eclipse.core.internal.events.BuildManager.basicBuildLoop(BuildManager.java:371)
    	at org.eclipse.core.internal.events.BuildManager.build(BuildManager.java:392)
    	at org.eclipse.core.internal.resources.Workspace.buildInternal(Workspace.java:515)
    	at org.eclipse.core.internal.resources.Workspace.build(Workspace.java:412)
    	at com.ti.ccstudio.project.core.services.ProjectBuilder.internalBuildProjects(ProjectBuilder.java:394)
    	at com.ti.ccstudio.project.core.services.ProjectBuilder.buildProjects(ProjectBuilder.java:283)
    	at com.ti.ccstudio.debug.launch.CCSLaunchDelegate.buildForLaunch(CCSLaunchDelegate.java:444)
    	at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:834)
    	at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:719)
    	at org.eclipse.debug.internal.ui.DebugUIPlugin.buildAndLaunch(DebugUIPlugin.java:1017)
    	at org.eclipse.debug.internal.ui.DebugUIPlugin$2.run(DebugUIPlugin.java:1220)
    	at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)
    !SUBENTRY 2 org.eclipse.core.resources 4 273 2022-04-05 14:46:18.779
    !MESSAGE Problems encountered while deleting resources.
    !SUBENTRY 3 org.eclipse.core.resources 4 273 2022-04-05 14:46:18.779
    !MESSAGE Could not delete 'C:\Repo\Raymond_BT_IO_application\Release\Raymond_BT_IO_application.out'.
    !STACK 1
    org.eclipse.core.runtime.CoreException: Problems encountered while deleting files.
    	at org.eclipse.core.internal.filesystem.local.LocalFile.delete(LocalFile.java:142)
    	at org.eclipse.core.internal.resources.ResourceTree.internalDeleteFile(ResourceTree.java:313)
    	at org.eclipse.core.internal.resources.ResourceTree.standardDeleteFile(ResourceTree.java:799)
    	at org.eclipse.core.internal.resources.Resource.unprotectedDelete(Resource.java:1779)
    	at org.eclipse.core.internal.resources.Resource.delete(Resource.java:757)
    	at org.eclipse.core.internal.resources.Resource.delete(Resource.java:727)
    	at com.ti.ccstudio.project.core.internal.build.temp.BuildDescriptionManager.cleanGeneratedRebuildResources(BuildDescriptionManager.java:265)
    	at com.ti.ccstudio.project.core.internal.build.CCSMakefileGenerator.generateMakefiles(CCSMakefileGenerator.java:318)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.performMakefileGeneration(CommonBuilder.java:1010)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.performPrebuildGeneration(CommonBuilder.java:872)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:752)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:515)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:461)
    	at org.eclipse.core.internal.events.BuildManager$2.run(BuildManager.java:833)
    	at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:220)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:263)
    	at org.eclipse.core.internal.events.BuildManager$1.run(BuildManager.java:316)
    	at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:319)
    	at org.eclipse.core.internal.events.BuildManager.basicBuildLoop(BuildManager.java:371)
    	at org.eclipse.core.internal.events.BuildManager.build(BuildManager.java:392)
    	at org.eclipse.core.internal.resources.Workspace.buildInternal(Workspace.java:515)
    	at org.eclipse.core.internal.resources.Workspace.build(Workspace.java:412)
    	at com.ti.ccstudio.project.core.services.ProjectBuilder.internalBuildProjects(ProjectBuilder.java:394)
    	at com.ti.ccstudio.project.core.services.ProjectBuilder.buildProjects(ProjectBuilder.java:283)
    	at com.ti.ccstudio.debug.launch.CCSLaunchDelegate.buildForLaunch(CCSLaunchDelegate.java:444)
    	at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:834)
    	at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:719)
    	at org.eclipse.debug.internal.ui.DebugUIPlugin.buildAndLaunch(DebugUIPlugin.java:1017)
    	at org.eclipse.debug.internal.ui.DebugUIPlugin$2.run(DebugUIPlugin.java:1220)
    	at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)
    Contains: Could not delete: C:\Repo\Raymond_BT_IO_application\Release\Raymond_BT_IO_application.out.
    java.nio.file.FileSystemException: C:\Repo\Raymond_BT_IO_application\Release\Raymond_BT_IO_application.out: The process cannot access the file because it is being used by another process.
    
    	at sun.nio.fs.WindowsException.translateToIOException(Unknown Source)
    	at sun.nio.fs.WindowsException.rethrowAsIOException(Unknown Source)
    	at sun.nio.fs.WindowsException.rethrowAsIOException(Unknown Source)
    	at sun.nio.fs.WindowsFileSystemProvider.implDelete(Unknown Source)
    	at sun.nio.fs.AbstractFileSystemProvider.deleteIfExists(Unknown Source)
    	at java.nio.file.Files.deleteIfExists(Unknown Source)
    	at org.eclipse.core.internal.filesystem.local.LocalFile.internalDelete(LocalFile.java:223)
    	at org.eclipse.core.internal.filesystem.local.LocalFile.delete(LocalFile.java:140)
    	at org.eclipse.core.internal.resources.ResourceTree.internalDeleteFile(ResourceTree.java:313)
    	at org.eclipse.core.internal.resources.ResourceTree.standardDeleteFile(ResourceTree.java:799)
    	at org.eclipse.core.internal.resources.Resource.unprotectedDelete(Resource.java:1779)
    	at org.eclipse.core.internal.resources.Resource.delete(Resource.java:757)
    	at org.eclipse.core.internal.resources.Resource.delete(Resource.java:727)
    	at com.ti.ccstudio.project.core.internal.build.temp.BuildDescriptionManager.cleanGeneratedRebuildResources(BuildDescriptionManager.java:265)
    	at com.ti.ccstudio.project.core.internal.build.CCSMakefileGenerator.generateMakefiles(CCSMakefileGenerator.java:318)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.performMakefileGeneration(CommonBuilder.java:1010)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.performPrebuildGeneration(CommonBuilder.java:872)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:752)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:515)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:461)
    	at org.eclipse.core.internal.events.BuildManager$2.run(BuildManager.java:833)
    	at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:220)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:263)
    	at org.eclipse.core.internal.events.BuildManager$1.run(BuildManager.java:316)
    	at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:319)
    	at org.eclipse.core.internal.events.BuildManager.basicBuildLoop(BuildManager.java:371)
    	at org.eclipse.core.internal.events.BuildManager.build(BuildManager.java:392)
    	at org.eclipse.core.internal.resources.Workspace.buildInternal(Workspace.java:515)
    	at org.eclipse.core.internal.resources.Workspace.build(Workspace.java:412)
    	at com.ti.ccstudio.project.core.services.ProjectBuilder.internalBuildProjects(ProjectBuilder.java:394)
    	at com.ti.ccstudio.project.core.services.ProjectBuilder.buildProjects(ProjectBuilder.java:283)
    	at com.ti.ccstudio.debug.launch.CCSLaunchDelegate.buildForLaunch(CCSLaunchDelegate.java:444)
    	at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:834)
    	at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:719)
    	at org.eclipse.debug.internal.ui.DebugUIPlugin.buildAndLaunch(DebugUIPlugin.java:1017)
    	at org.eclipse.debug.internal.ui.DebugUIPlugin$2.run(DebugUIPlugin.java:1220)
    	at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)
    !SUBENTRY 4 org.eclipse.core.filesystem 4 273 2022-04-05 14:46:18.780
    !MESSAGE Problems encountered while deleting files.
    !SUBENTRY 5 org.eclipse.core.filesystem 4 273 2022-04-05 14:46:18.780
    !MESSAGE Could not delete: C:\Repo\Raymond_BT_IO_application\Release\Raymond_BT_IO_application.out.
    !STACK 0
    java.nio.file.FileSystemException: C:\Repo\Raymond_BT_IO_application\Release\Raymond_BT_IO_application.out: The process cannot access the file because it is being used by another process.
    
    	at sun.nio.fs.WindowsException.translateToIOException(Unknown Source)
    	at sun.nio.fs.WindowsException.rethrowAsIOException(Unknown Source)
    	at sun.nio.fs.WindowsException.rethrowAsIOException(Unknown Source)
    	at sun.nio.fs.WindowsFileSystemProvider.implDelete(Unknown Source)
    	at sun.nio.fs.AbstractFileSystemProvider.deleteIfExists(Unknown Source)
    	at java.nio.file.Files.deleteIfExists(Unknown Source)
    	at org.eclipse.core.internal.filesystem.local.LocalFile.internalDelete(LocalFile.java:223)
    	at org.eclipse.core.internal.filesystem.local.LocalFile.delete(LocalFile.java:140)
    	at org.eclipse.core.internal.resources.ResourceTree.internalDeleteFile(ResourceTree.java:313)
    	at org.eclipse.core.internal.resources.ResourceTree.standardDeleteFile(ResourceTree.java:799)
    	at org.eclipse.core.internal.resources.Resource.unprotectedDelete(Resource.java:1779)
    	at org.eclipse.core.internal.resources.Resource.delete(Resource.java:757)
    	at org.eclipse.core.internal.resources.Resource.delete(Resource.java:727)
    	at com.ti.ccstudio.project.core.internal.build.temp.BuildDescriptionManager.cleanGeneratedRebuildResources(BuildDescriptionManager.java:265)
    	at com.ti.ccstudio.project.core.internal.build.CCSMakefileGenerator.generateMakefiles(CCSMakefileGenerator.java:318)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.performMakefileGeneration(CommonBuilder.java:1010)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.performPrebuildGeneration(CommonBuilder.java:872)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:752)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:515)
    	at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:461)
    	at org.eclipse.core.internal.events.BuildManager$2.run(BuildManager.java:833)
    	at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:220)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:263)
    	at org.eclipse.core.internal.events.BuildManager$1.run(BuildManager.java:316)
    	at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
    	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:319)
    	at org.eclipse.core.internal.events.BuildManager.basicBuildLoop(BuildManager.java:371)
    	at org.eclipse.core.internal.events.BuildManager.build(BuildManager.java:392)
    	at org.eclipse.core.internal.resources.Workspace.buildInternal(Workspace.java:515)
    	at org.eclipse.core.internal.resources.Workspace.build(Workspace.java:412)
    	at com.ti.ccstudio.project.core.services.ProjectBuilder.internalBuildProjects(ProjectBuilder.java:394)
    	at com.ti.ccstudio.project.core.services.ProjectBuilder.buildProjects(ProjectBuilder.java:283)
    	at com.ti.ccstudio.debug.launch.CCSLaunchDelegate.buildForLaunch(CCSLaunchDelegate.java:444)
    	at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:834)
    	at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:719)
    	at org.eclipse.debug.internal.ui.DebugUIPlugin.buildAndLaunch(DebugUIPlugin.java:1017)
    	at org.eclipse.debug.internal.ui.DebugUIPlugin$2.run(DebugUIPlugin.java:1220)
    	at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)
    
    !ENTRY com.ti.ccstudio.debug 1 0 2022-04-05 14:49:22.776
    !MESSAGE DS_ERROR: Cortex_M4_0: JTAG Communication Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.4.0.00129) 
    
    
    !ENTRY com.ti.ccstudio.debug 1 0 2022-04-05 14:49:23.099
    !MESSAGE DS_ERROR: Cortex_M4_0: Failed to remove the debug state from the target before disconnecting.  There may still be breakpoint op-codes embedded in program memory.  It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
    
    

  • Thanks James.

    Could you also provide a screenshot of the entire CCS IDE with the blank ROV view?

    Thanks

    ki

  • Engineering took a look at the log and does not see anything in there related to ROV.

    Would it be possible to share the *.out file that you are loading? You can share via private E2E message if you do not want to post it publicly.

    Thanks

    ki

  • Sure lemme send it to you private