Hi
I am missing an obvious feature in CCS,
Use case:
Very often when I have made changes to the sysconfig.syscfg file, I just want to run the generation of the sysconfig files, not building the whole project. fx. to see how a new define in board.h now looks like, So i can update my code accordingly.
Suggestion:
In CCS we alreade have the posibility to right click on a .c file and select "build Selected Files(s)", and it will trigger a build of just that file Well I also have that option when right clicking on the .syscfg file, just nothing happens when I select it.
So I suggest that selecting "build Selected Files(s)" on a .syscfg file triggers the sysconfig generation.
More specifically runs this step only
Building file: "../modtager.syscfg" Invoking: SysConfig "C:/ti/ccs1110/ccs/utils/sysconfig_1.11.0/sysconfig_cli.bat" -s "C:/ti/c2000/C2000Ware_4_00_00_00/.metadata/sdk.json" --script "C:/somepath/somename.syscfg" -o "syscfg" --compiler ccs Running script... Validating... Generating Code (modtager.syscfg)... Writing C:\somepath\SomeConfig\syscfg\board.c... Writing C:\somepath\SomeConfig\syscfg\board.h... Writing C:\somepath\SomeConfig\syscfg\pinmux.csv... Finished building: "../somename.syscfg"