Part Number: CODECOMPOSER
Other Parts Discussed in Thread: TMS320F280045, TMDSCNCD280049C, C2000WARE
Dear Sirs
I'm developing code for the TMS320F280045 uC. I need to have SPI master and slave communication abilities. I have experience with the TIVA series controller but none with the C2000 series controller. To get familiar with the C2000 series controller, I purchased the TMDSCNCD280049C control board and the TMDSHSEDOCK docking station. To understand the SPI, I open the spi_ex3_external_loopback project in the following folder, C:\TI\c2000\C2000Ware_4_00_00_00\driverlib\f28004x\examples\spi. I typically open each of the init functions to see how the controller and the peripheral are initialized. I do this before compiling. When I try to open the Board_init() function, I cannot find the source code. I did a search, but found only .c.xdt and .h.xdt files. However, after compiling the the project I can open the Board_init() function source code and header in their respective files. I assume these files are generated at compile time. I notice there is a .syscfg file included when I open the project. I haven't been able to find any documentation on this process. Please help me on this issue. Thank you.