This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Import CCS project issue

Hello everyone,

I need to import a CCS project released with the CCS version 10.1.0.00010

I have installed the CCS 10.1.0.00010

When I try to import the project, the following error appears:

See details below... 
 bleSSS_wmbus169_cc2640r2_app
  Product com.ti.SIMPLELINK_CC2640R2_SDK v2.40.0.32 is not currently installed and no compatible version is available. Please install this product or a compatible version.

 

I have downloaded and installed the CC2640R2_SDK v2.40.0.32.

I have tried again but the error is the same.

Here there is the screenshot of the issue.

Thanks!

Massimo