Part Number: CODECOMPOSER
Other Parts Discussed in Thread: TM4C1294NCPDT
I have just bought two XDS110 Debug Probes
Before moving to Code Composer 11 I decided to make sure my code was running in Code Composer 6.
Both devices were detected in 11.
When I setup the debug target configuration as a XDS110, I previously used a XDS510 and then tested the connection the probes disconnected and never came back.
Both probes are now not recognised in device manager and Code Composer 6 or 11
Running "xdsdfu -e" returns with both devices not found.
When plugged in the D1 LED is lit but no USB connection.
Did testing the connection blow both devices !!