Other Parts Discussed in Thread: CC1352P
Hi Experts,
I tried to execute the Pin interrupt CC1352P example in LInux Os enviroment.
I'm getting isuse on debug session IcePick_C: Error initializing emulator: (Error -260 @ 0x0).
Can anyone help me to overcome this issue !
The following error screenshot:

While verify the connection in the general.. I'm getting this
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
/home/keerthivasan/.ti/ccs1120/1/0/BrdDat/
testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100/110/510 class product.
This utility will load the adapter 'libjioxds110.so'.
The library build date was 'Mar 17 2022'.
The library build time was '15:40:16'.
The library package version is '9.7.0.00213'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-260' (0xfffffefc).
The title is 'SC_ERR_XDS110_OPEN'.
The explanation is:
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the XDS110SupportReadMe.pdf
file there for instructions.
[End]