This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Code Composer Studio (CCS11.2.0.00007) Error On Fresh Install

Hi Everyone, 
I hope all is well. I am currently having issues with installing Code Composer Studio version CCS11.2.0.00007, and was wondering if anyone has seen the following issue before?

The installer works great up until the final steps. It seems to have issues with the emupack installer. 

The CCS installer brings up a warning prompt that the emupack installer exited with an error code. I did do some digging, and pulled up the error log for the emu pack installer and found the following information:

Error copying file from packed archive C:/Users/kuhnst/AppData/Local/Temp/CCS_E2~1/EMU_TI/TI_EMU~1.EXE to C:/ti/ccs1120/ccs/ccs_base/emulation/analysis/bin/SCDecoderUnit.dll
There has been an error.
Unable to copy file
Exiting with code 1

I have a hunch that there may be a permissions issue with the installer, but wanted to get someone elses input on it. I am unsure if this helps, 

but I did try rebooting my computer and trying again. 

I also tried force running the installer as admin to see if that would help, with no luck as well.