I use CCS4 for MSP430 developments and now intend to also use it for Piccolo and Stellaris. I do not use it for high end DSP.
Today I attempted to update CCS4. It downloaded all files (approximately 300 MB) successfully.
Then it throws error:
My Computer configuration:
CCS4: Node locked license, CPU: i5-760, OS: Windows 7 (32bit), RAM 4GB (Usable 3.16 GB), NVIDIA graphics card, 1 TB Seagate Harddisk. CCS4 installed at default locations.
All installed software, except CCS4 update, are working fine. Even CCS4 existing installation is also working fine. Only issue is happening during update.
All retries give same error message. If I quit CCS4 and start again, all download starts from beginning. At the end, it throws same error message again.
Why can't CCS4 retain what it has downloaded (until it is satisfactorily installed)? What do I do to get rid of the above error? Please help.
TI needs to enhance few things about this (otherwise fairly good) compiler, especially deal with mountain-sized updates which unluckily fail only at the end and vanish from the hard drive. Honestly, I have spent more time in wrestling with CCS4 (and its updates) for past few months than the time I could fruitfully spend on my application code itself. The compiler itself seems fairly good, probably because it is GCC internally (and uses Eclipse IDE). My appreciations to TI team for the stable operation of the CCS4 compiler/ide.
Thanks in advance for the help.
Regards.
Suresh Joshi (suresh_b_joshi@yahoo.com)