Hello,
I upgraded from Fedora 35 to Fedora 36 and now CCS refuses to launch. Under Fedora 35 everything worked fine. I tested with a fresh install of the newest CCS version (11.2).
The error is logged in a file (attached) and boils down to the following:
java.lang.UnsatisfiedLinkError: Could not load SWT library. Reasons:Can't load library: ~/swt/lib/linux/x86_64/libswt-pi4-gtk.so
This seems to be an eclipse problem. I found the discussion [1] and several similar posts, none of which could solve my problem.
Any ideas on how to tackle this?
Convenience warning: I'll be offline until next week shortly.
Thanks in advance
!SESSION 2022-05-25 11:52:16.634 ----------------------------------------------- eclipse.buildId=4.19.0.I20210303-1800 java.version=11.0.13 java.vendor=Eclipse Adoptium BootLoader constants: OS=linux, ARCH=x86_64, WS=gtk, NL=de_DE Framework arguments: -product com.ti.ccstudio.branding.product Command-line arguments: -os linux -ws gtk -arch x86_64 -product com.ti.ccstudio.branding.product !ENTRY org.eclipse.osgi 4 0 2022-05-25 11:52:17.569 !MESSAGE Application error !STACK 1 java.lang.UnsatisfiedLinkError: Could not load SWT library. Reasons: no swt-pi4-gtk-4942r22 in java.library.path: [/home/markus/ti/ccs1120/ccs/eclipse/jre/lib/server, /home/markus/ti/ccs1120/ccs/eclipse/jre/lib, ., /usr/java/packages/lib, /usr/lib64, /lib64, /lib, /usr/lib] no swt-pi4-gtk in java.library.path: [/home/markus/ti/ccs1120/ccs/eclipse/jre/lib/server, /home/markus/ti/ccs1120/ccs/eclipse/jre/lib, ., /usr/java/packages/lib, /usr/lib64, /lib64, /lib, /usr/lib] Can't load library: /home/markus/.swt/lib/linux/x86_64/libswt-pi4-gtk-4942r22.so Can't load library: /home/markus/.swt/lib/linux/x86_64/libswt-pi4-gtk.so at org.eclipse.swt.internal.Library.loadLibrary(Library.java:338) at org.eclipse.swt.internal.Library.loadLibrary(Library.java:257) at org.eclipse.swt.internal.gtk.OS.<clinit>(OS.java:96) at org.eclipse.swt.internal.Converter.wcsToMbcs(Converter.java:209) at org.eclipse.swt.internal.Converter.wcsToMbcs(Converter.java:155) at org.eclipse.swt.widgets.Display.<clinit>(Display.java:163) at org.eclipse.ui.internal.Workbench.createDisplay(Workbench.java:726) at org.eclipse.ui.PlatformUI.createDisplay(PlatformUI.java:168) at org.eclipse.ui.internal.ide.application.IDEApplication.createDisplay(IDEApplication.java:182) at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:125) at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255) at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method) at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(Unknown Source) at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source) at java.base/java.lang.reflect.Method.invoke(Unknown Source) at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:653) at org.eclipse.equinox.launcher.Main.basicRun(Main.java:590) at org.eclipse.equinox.launcher.Main.run(Main.java:1461)