Part Number: CODECOMPOSER
Other Parts Discussed in Thread: TMS320F28379D
Hi TI Expert Team,
With reference to : CLA Hands On Workshop - Part 3 The Workshop | TI.com Video,
we would like to try it out on TMS320F28379D Launchpad.
Using CCS version 10.4..0.00006, we were getting error when trying to open a single time Graph in Javascript
with the Scripting Console using an absolute path in the second argument : openAnalysisView('Single Time','C:/ti/CLA_HandsOnWorkshop_Camtasia2017/solution/ccs/fft_mag.graphProp')
js:> loadJSFile "C:\ti\CLA_HandsOnWorkshop_Camtasia2017\solution\ccs\SetupDebugEnv.js"
java.lang.IllegalArgumentException: Illegal secondary id (cannot be empty or contain a colon) (C:\ti\ccs104\ccs\eclipse\configuration\org.eclipse.osgi\481\0\.cp\resources\dvtviews.js#131)
===> [Comment] : wondering how to specify the absolute path without having a colon for the drive such as "C:"
Because of the error, we then move the "SetupDebugEnv.js" and "fft_mag.graphProp" to the CCS project workspace and modify the second argument
to use relative, instead of absolute, path of openAnalysisView to : openAnalysisView('Single Time', 'fft_mag.graphProp').
But again this does not make the error go away. The system returned with a new error saying :
js:> loadJSFile "C:\Users\rrntuguest\workspace_v100\F28379D_CLAHandsOn_Solution\SetupDebugEnv.js"
java.lang.IllegalArgumentException: Illegal view mode (C:\ti\ccs104\ccs\eclipse\configuration\org.eclipse.osgi\481\0\.cp\resources\dvtviews.js#131)
===> Up to this point, we do not know what to do and how to change the view mode. Can someone advise a remedy please ?
Thinking maybe the bug (if there was) will have been fixed in the latest version of CCS, so we upgraded our CCS from version 10.4.0.00006 to
CCS version 11.2.0.00007.
However, the latest version also does not free from error. It gave another new error saying :
When running the Scripting Console and using the function openAnalysisView('Single Time','C:/fft_mag.graphProp') I get following error:
ReferenceError: "GSSScripting" is not defined. (C:\ti\c2000\ccs1120\ccs\eclipse\configuration\org.eclipse.osgi\139\0\.cp\resources\dvtviews.js#130)
Apparently, this new error had been reported by somebody else and was seen in version 11.0 and 11.1, but so far had received no fixed.
We want to see the CLA in the workshop working and we do not care about the CCS version so long it is working.
Can someone advise a fix for "illegal view mode" or at least which CCS version was used for the CLA workshop ?
Thank you and looking forward to receiving further advice on the remedy.
Djony Pamudji