This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB560 v2 System Trace

Hello,

 I use several Blackhawk USB560v2 debuggers and most of the times facing no issue with them.

 

Suddenly one of those devices neither completes the boot sequence nor enters the Safe Mode (even after switching it on and off during short intervals for at least 20 times).

On the contrary, the ‘USB’ LED remains constantly red all the time while the ‘MODE’ LED blinks green for at least an hour that it remained plugged to the USB port.

 

All the other devices function correctly using the same Usb cable, the same Usb port in the same computer.

Do you have any suggestions for solving this issue ?

 

Yours sincerely