Hello,
I just performed a silent installation of Code Composer Studio 9.3 on Windows Server 2019. The installation is ok.
The command used for the installation is the following one:
C:\Users\myuser\Documents\Software\ccs_setup_9.3.0.00012.exe --prefix C:\Tools\CCS9 --mode unattended
But when I run the application, I have this error message:
An error has occured, see the log file null.
What is the fix for this problem?
Is there a recommended version of Code Composer Studio for Windows Server 2019?
Thanks