Hi,
I wish to have a running graph of a data. CCS 4 has option for displaying Graph. However i wish to create my own application.
I know the basics of debugging, but i have no idea of GEL/DSS/Java Scripting. For starters, please help me how to do the following in JS.
1) I have a interrupt running at 40us in 28035 processor. I wish to acquire the value at address '0x000---' every 40us.
2) Store the data acquired in a temporary buffer of length 1024 ( external to 28035 in some array).
3) Once 1024 samples are acquired, dump 1024 values into a .csv file with time stamp/sample number.
Thanks.
with warm regards,
K.Sugantha