I am considering L138 for a telecom project. I have C6 and DSP/BIOS experience, but no ARM or dual-core experience.
Can the ARM core be set up to operate under SYS/BIOS?
Can I set up SYS/BIOS on both the ARM core and the C6 core in order to send message between threads on the different processors (e.g. shared semaphore or ARM-post / C6-pend)?
Can I set up CCS to single-step debug both ARM and C6 cores at the same time over the single JTAG connection?
Is the CCS that comes with the Experimenter kit fully functional except for the restriction to that specific board?
Do any of the TI CODEC libraries include G.729?
Are the additional capabilities of the XDS560 over the XDS510 relevant to the L138?
Can you point me to an application note that discusses communication between the cores?