Other Parts Discussed in Thread: CODECOMPOSER, TMS320F28335
Hello, I am using a eZdspF28335 board and I am having connectivity problems. It was working fine for some time. Sometimes it lost connection during debbuging, but I was able to connect again to it. Nowadays, every time I try to connect to it, I get this message on CodeComposer:
Error connecting to the target:
Error 0x80000200/-1135
Fatal Error during: OCS,
Unrecoverable emulation error
The onboard emulator is recognized by CodeComposer and is USB enumerated. I am running CodeComposer on Windows (both XP and Vista), and the board appears on Device Manager every time I connect it. Apparently, the hardware seems to be working fine.
The first time this problem ocurred I was running CodeComposer 4 on Windows Vista. While I was trying to figure out the problem, I found that I was able to connect to the board using another computer, running CodeComposer 3.3 on Windows XP. But, after three weeks it also started to show problems. The last time I was able to connect, I could load and debug a program, but the connection was lost after some time and I never could connect again.
First of all, what does "Error 0x80000200/-1135" mean?