Part Number: CCSTUDIO-SITARA
Other Parts Discussed in Thread: SYSCONFIG
Hi,
I'm attempting to create a new CCS project from scratch and I want it to have a sysconfig configuration. I was surprised to find there's no option to do that, at least not that I've found. The only way I've been able to get a sysconfig project is to import an existing project that has already has sysconfig in it. For example, I was able to import one from the MCU+ SDK for AM24xx.
BTW, as an experiment, I created a sysconfig project on the cloud at dev.ti.com and saved off the .syscfg file. I then tried adding that .syscfg file to a basic CCS project I created and ran into issues. Probably could have resolved them with some effort but decided that's not really the approach I want to pursue.
I guess importing a project that's close to what I want as a starting point is okay but many times, I just like to create a new project from scratch.
I have two questions
1) Am I missing something or importing an existing project is the only feasible way?
2) I haven't downloaded CCS12 yet, does it allow me to do this? I want to check first before doing the big download/install.
Thanks