This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am currently running a custom board with OMAP L138 and XDS100 emulator. With a gel script. I am running into a error shown below
ARM9_0: GEL: Error while executing OnTargetConnect(): Target failed to write memory at 0x01C11100.
If I comment the code out, it throws an error for the same memory location. The Gel script is a modified one from Logic PD. This error shows up in the
device_PLL0() method.
The register that the emulator cannot write to is PLL0_PLLCMD. Below is a portion of the gel. \
This only happens when using a xds100V2. It runs smoothly when using a xds510.
I appreciate any help.
device_PLL0(unsigned int CLKMODE, unsigned int PLLM, unsigned int POSTDIV,unsigned int PLLDIV1, unsigned int PLLDIV2, unsigned int PLLDIV3, unsigned int PLLDIV7 ) {
unsigned int i=0;
/* Clear PLL lock bit */
CFGCHIP0 &= ~(0x00000010);
/* Set PLLENSRC '0',bit 5, PLL Enable(PLLEN) selection is controlled through MMR */
PLL0_PLLCTL &= ~(0x00000020);
/* PLLCTL.EXTCLKSRC bit 9 should be left at 0 for Freon */
PLL0_PLLCTL &= ~(0x00000200);
/* Set PLLEN=0 to put in bypass mode*/
PLL0_PLLCTL &= ~(0x00000001);
/*wait for 4 cycles to allow PLLEN mux switches properly to bypass clock*/
for(i=0; i<PLLEN_MUX_SWITCH; i++) {;}
/* Select the Clock Mode bit 8 as External Clock or On Chip Oscilator*/
PLL0_PLLCTL &= 0xFFFFFEFF;
PLL0_PLLCTL |= (CLKMODE << 8);
/*Clear PLLRST bit to reset the PLL */
PLL0_PLLCTL &= ~(0x00000008);
/* Disable the PLL output*/
PLL0_PLLCTL |= (0x00000010);
/* PLL initialization sequence
Power up the PLL by setting PWRDN bit set to 0 */
PLL0_PLLCTL &= ~(0x00000002);
/* Enable the PLL output*/
PLL0_PLLCTL &= ~(0x00000010);
/*PLL stabilisation time- take out this step , not required here when PLL in bypassmode*/
for(i=0; i<PLL_STABILIZATION_TIME; i++) {;}
/*Program the required multiplier value in PLLM*/
PLL0_PLLM = PLLM; /* Make PLLMULTIPLEIR as bootpacket*/
/* Prediv setup -Not required */
// PLL0_PREDIV = 0x8000 | PREDIV; /* Make POSTDIV as bootpacket*/
/*If desired to scale all the SYSCLK frequencies of a given PLLC, program the POSTDIV ratio*/
PLL0_POSTDIV = 0x8000 | POSTDIV; /* Make POSTDIV as bootpacket*/
/*Check for the GOSTAT bit in PLLSTAT to clear to 0 to indicate that no GO operation is currently in progress*/
while(PLL0_PLLSTAT & 0x1==1){}
/*Program the RATIO field in PLLDIVx with the desired divide factors. In addition, make sure in this step you leave the PLLDIVx.DxEN bits set so clocks are still enabled (default).*/
PLL0_PLLDIV1 = 0x8000 | PLLDIV1; /* Make PLLDIV1 as bootpacket, do it for other PLLDIVx to if required*/
PLL0_PLLDIV2 = 0x8000 | PLLDIV2;
PLL0_PLLDIV4 = 0x8000 | (((PLLDIV1+1)*4)-1);
PLL0_PLLDIV6 = 0x8000 | PLLDIV1;
PLL0_PLLDIV3 = 0x8000 | PLLDIV3; /* Make PLLDIV3 as bootpacket, do it for other PLLDIVx to if required*/
PLL0_PLLDIV7 = 0x8000 | PLLDIV7; /* Make PLLDIV7 as bootpacket, do it for other PLLDIVx to if required*/
/*Set the GOSET bit in PLLCMD to 1 to initiate a new divider transition.*/
PLL0_PLLCMD |= 0x1;
/*Wait for the GOSTAT bit in PLLSTAT to clear to 0 (completion of phase alignment).*/
while(PLL0_PLLSTAT & 0x1==1) { }
/*Wait for PLL to reset properly. See PLL spec for PLL reset time - This step is not required here -step11*/
for(i=0; i<PLL_RESET_TIME_CNT; i++) {;} /*128 MXI Cycles*/
/*Set the PLLRST bit in PLLCTL to 1 to bring the PLL out of reset*/
PLL0_PLLCTL |= 0x8;
/*Wait for PLL to lock. See PLL spec for PLL lock time*/
for(i=0; i<PLL_LOCK_TIME_CNT; i++) {;} /*Make PLL_LOCK_TIME_CNT as boot Packet*/
/*Set the PLLEN bit in PLLCTL to 1 to remove the PLL from bypass mode*/
PLL0_PLLCTL |= 0x1;
/* SET PLL lock bit*/
CFGCHIP0 |= (0x1 << 4) & 0x00000010;
}
-Manas
Ki-Soo Lee said:
This requires a Clear Quest login. This probably is internal to TI. Could you please give me an update on this issue?
-Manas
Sorry, try this link:
So far I can see that this bug is still under review.
Thanks
ki