This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fill Linker Output With 0xFF

Our standard is to fill unused code space with 0xFF.  Under the Code Composer Studio v4 project properties for C/C++ Build, under Tool Settings, under MSP430 Linker I found "Runtime Environment" which had "Default fill value for holes in output sections (--fill_value, -f)" and thought this is what I need, but it doesn't work or I don't understand how it works.  I placed a 0xFF in the field recompiled and linked and it did NOT fill open space with 0xFF.  I also tried 255, but that did not work.  I thought maybe I had to add the '-f", but then the linker complained the value was negative.

We are creating an Intel Hex output.  When I look at the resultant output it does not contain 0xFF fill.   

What am I doing wrong?

Thanks

John Aggers

Emerson Climate Technologies

770-425-2724